Getting started with embedded metering applications using MSP430i20xx MCUs
Start developing your power or energy measurement with this virtual bundle, and see the required hardware, software, example code, demos and key documentation.
评估板
EVM430-I2040S — 用于辅助计量的 MSP430I240 评估板
TI.com 上无现货
TI.com 上无现货
开发套件
MSP-EXP430F5529LP — MSP430F5529 LaunchPad™ development kit for USB
Jumper wires are required but do not come with this kit.
TI.com 上无现货
子卡
MSP-ISO — 适用于 MSP LaunchPad 开发套件的隔离适配器
Jumper wires are required but do not come with this kit.
TI.com 上无现货
软件编程工具
UNIFLASH — 适用于大多数 TI 微控制器 (MCU) 和毫米波传感器的 UniFlash
UNIFLASH — 适用于大多数 TI 微控制器 (MCU) 和毫米波传感器的 UniFlash
版本: 8.6.0
发布日期: 07 二月 2024
校验和
校验和
校验和
产品
C2000 实时微控制器
基于 Arm 的处理器
工业毫米波雷达传感器
汽车毫米波雷达传感器
MSP430 微控制器
Wi-Fi 产品
Arm Cortex-M4 MCU
Arm Cortex-M0+ MCU
Arm Cortex-R MCU
低功耗 2.4GHz 产品
汽车类无线连接产品
Sub-1GHz 无线 MCU
发布信息
UniFlash is a standalone tool used to program on-chip and external flash memory on TI MCUs and on-board flash memory for Sitara processors. UniFlash has a GUI, command line, and scripting interface. UniFlash is available free of charge.
最新信息
- Device Support Update
- Synced up with CCS12.6.0 and CCS Theia 1.3.0
- Fixed issues with loading the MSPM0 Bootloader flash library
- Bug Fixes
应用软件和框架
MSP430-ENERGY-MEASUREMENT — 适用于具有 24 位 Σ-Δ ADC 的 MSP430 MCU 的电能测量库
MSP430-ENERGY-MEASUREMENT — 适用于具有 24 位 Σ-Δ ADC 的 MSP430 MCU 的电能测量库
版本: 1.40.00.03
发布日期: 29 七月 2020
Windows Installer for Energy Measurement Design Center
校验和
macOS Installer for Energy Measurement Design Center
校验和
Linux Installer for Energy Measurement Design Center
校验和
产品
MSP430 微控制器
硬件开发
评估板
开发套件
子卡
文档
Energy Measurement Design Center Technology Guide
Energy Measurement Design Center API Guide
发布信息
The Energy Measurement Design Center is a rapid development tool that enables energy measurement using TI MSP430i20xx and MSP430F67xx Flash-based microcontrollers (MCUs). It includes a graphical user interface (GUI), documentation, software library and examples that can simplify development and accelerate designs for power monitoring and energy measurement in smart grid and building automation applications. Start by dragging and dropping a MCU, voltage sensors, and current sensors into the GUI workspace. Configure the MCU and each sensor according to your system configuration. The GUI will check for errors before generating the source code. Import the code into an IDE and program the MCU. The GUI will allow you to easily calibrate the device and view the results.
最新信息
- Software
- Fixed an issue where the MSP430i20xx OSR (sampling rate) did not change from the default value.
- Removed duplicate hal_system_Init() call.
- Re-initialized results after disabling interrupts and writing calibration factors to INFO memory.
- Re-calibrated MSP430i20xx EMDC example projects and firmware images.
- Technology Guide
- Included a flowchart for the EMDC application code including foreground and background processes.
- Added a Known Limitations section to the Introduction for more awareness.
- Fixed the Result Parameter command values in the Commands from Target to EMDC section and sequence diagrams.
- Added more details about the packet structure and checksum calculation in the Communication Protocol Spec section.
- Included the default UART communication settings.
- Updated the EMDC start-up image to fix a broken pixel in the platform bar.
- Fixed some minor formatting issues.