LP-MSPM0C1104 是一款原型评估模块,限量出售
LP-MSPM0C1104
适用于 24MHz Arm® Cortex®-M0+ MCU 的 MSPMC1104 LaunchPad™ 开发套件
LP-MSPM0C1104
概述
LP-MSPM0C1104 LaunchPad™ 开发套件是基于 MSPM0C1104 的易用型评估模块 (EVM),包含在 MSPM0C1104 M0+ MCU 平台上开始开发所需的全部资源,包括用于编程和调试的板载调试探针,并且外形尺寸更小。该板包含两个按钮和一个 LED。
特性
- 板载调试器 probeRed LEDUser 输入按钮
- 红光 LED
- 用户输入按钮
Arm Cortex-M0+ MCU
立即订购并开发
LP-MSPM0C1104 — MSPM0C1104 24MHz Arm Cortex-M0+ MCU LaunchPad 开发套件
MSP-GANG-SOFTWARE — MSP-GANG 软件
MSP-GANG-SOFTWARE — MSP-GANG 软件
MSP-GANG Installer 1.03.09.00
产品
Arm Cortex-M0+ MCU
MSP430 微控制器
硬件开发
评估板
开发套件
文档
MSP-GANG Manifest
发布信息
The MSP Gang Programmer is a MSPM0/MSP430/MSP432 device programmer that can program up to eight identical flash or FRAM devices at the same time. The MSP Gang Programmer connects to a host PC using a standard RS-232 or USB connection and provides flexible programming options that allow the user to fully customize the process.
The MSP Gang Programmer is provided with an expansion board, called the Gang Splitter, that implements the interconnections between the MSP Gang Programmer and multiple target devices. Eight cables are provided that connect the expansion board to eight target devices (via JTAG or Spy-Bi-Wire connectors). The programming can be done with a PC or as a standalone device. A PC-side Graphical User Interface is also available and is DLL-based.
Features:
- Quickly and reliably program Flash or FRAM-based MSP devices via an RS-232 or USB interface
- Several programming modes:
- Interactive Mode Programming while connected to PC using the MSP GANG Programmer GUI
- Program from Image: An image can be stored, which contains configuration options and code files. This allows users to program MSP devices standalone, without a PC
- Programming from Script: Enables developers to automate more complicated programming procedures.
- Intuitive GUI for configuring, programming and testing production setup
- SD Card slot for storing images
- LCD screen for easy programming without a PC
- Supports up to 8 targets simultaneously
- Supports MSPM0/MSP430/MSP432 devices
最新信息
- Added low-power mode debug support for MSPM0
MSPM0-SDK — MSPM0 Software Development Kit (SDK)
MSPM0 SDK for Windows
MSPM0 SDK for macOS
MSPM0 SDK for Linux
产品
Arm Cortex-M0+ MCU
硬件开发
评估板
文档
MSPM0 SDK Documentation Overview
MSPM0 SDK Manifest
发布信息
The MSPM0 SDK delivers components that enable engineers to develop applications on Texas Instruments MSPM0 microcontroller devices. The product is comprised of multiple software components and more than 150 examples of how to use these components together. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.
The MSPM0 SDK includes support for FreeRTOS and a wide variety of middleware and drivers, including:
- Support for MSPM0L11xx/L13xx, MSPM0G1x0x/G3x0x, MSPM0C110x, MSPS003FX, and MSPM0L122X/L22X
- DriverLib with optimized footprint and performance
- Motor control examples for Stepper, Brushed, Sensorless FOC, and Hall Sensored Trap
- EEPROM emulation library
- IQMath for fixed point math
- Boot Image Manager to add secure booting features
- Libraries and demos for multiple protocols, including DALI, SMBus, PMBus, 1-Wire, etc.
- and more...
The MSPM0 MCU portfolio offers a single development environment that delivers flexible hardware, software and tool options for customers developing applications. A one-time investment with the MSPM0 software development kit (SDK) allows you create portable and modular code, opening the door to create unlimited applications.
最新信息
- Fixed issue with selecting mux mode in DL_LCD_setPinAsCommon API
- Fixed MCAN peripheral not being available for the MSPM0G310X devices in SysConfig
- Refer to the Release Notes for more details
CCSTUDIO-THEIA — Code Composer Studio™ integrated development environment (IDE) Theia
CCSTUDIO-THEIA — Code Composer Studio™ integrated development environment (IDE) Theia
产品
Arm Cortex-M0+ MCU
Sub-1GHz 无线 MCU
汽车类无线连接产品
低功耗 2.4GHz 产品
其他无线产品
MSP430 微控制器
C2000 实时微控制器
Arm Cortex-R MCU
基于 Arm 的处理器
汽车毫米波雷达传感器
工业毫米波雷达传感器
硬件开发
评估板
发布信息
Bug Fixes
- XDS110 serial number could be corrupted on a split launchpad
- Many build and project system related improvements.
Known Issues
- Decoding of core trace data may take up to 20 seconds for large captures. Performance can be improved 2x - 3x by performing the following actions:
- Right click on the core and select "Show all cores" from the context menu
- Select the new visible node which is called "DebugCell_TBR_0"
- Right click on that node and select "Connect Target"
- PC Hibernation affects CCS Theia inter-process communication with Resource Explorer opened. You may see a message “Error communicating with Cloud Agent “. Also, a notification panel in bottom right will be shown indicating that CCS Theia has gone offline. Please choose Restart option to restart CCS Theia and re-establish IPC communication.
General Information
- New Theia-IDE based IDE:
- Simple, easy-to-use environment
- Compatible with VS Code® extensions:
- You may need to configure proxy settings to access open-vsx.org where Theia enabled extensions are hosted.
- Source code navigation.
- Debug views such as breakpoints, callstack, variables, registers, memory and graphs.
- Target Configuration View
- Project-less debug support
- New features are being added with every release, please check What’s New section for details.
Compatibility:
- Project System is fully compatible with existing Code Composer Studio projects, meaning that existing projects (or example projects in SDKs) can be imported into CCS Theia. Workspaces are not compatible.
- Simply import your existing projects or examples from the SDK and get started
- Debug: Project based debugging is supported by providing same single click Debug Active Project action as in CCS 12.x. Project-less debug, ability to start a debug session from target configuration file (ccxml) is supported.
- Workspace: CCS Theia is using different underlying framework as such workspaces are not compatible between CCS products based on Eclipse. However, projects are fully compatible.
- CCS Theia supports ability to open a folder that holds CCS Projects or open a folder where projects should reside.
- Similar to VS Code, CCS Theia can open multiple distinct folders that hold projects. This is documented in VS Code as multi-root workspace. However, project names need to be unique across different folders.
Compilers
- TI CLANG 3.2.2 LTS, C2800 Compiler Tools v22.6.1 and MSP430 Compiler Tools v21.6.1.LTS compilers are bundled
Device Support
- Recommended for production development: MSPM0, MSP430, Wireless connectivity, Sitara MCU, mmWave
- Evaluation, not recommended for production development: Sitara MPU, Jacinto
最新信息
- Update to Theia v1.46 baseline
- Improvements in trace support
- Energy Trace ++ support for MSP430
- System Project debug with OptiShare
- Breakpoint view improvements
- Register view improvements
- Real time view updates
- MSPM0 Wait-in-reset support
- ARM Core Trace
LP-MSPM0C1104-OOBE — Out-of-box experience GUI for LP-MSPM0C1104
产品
Arm Cortex-M0+ MCU
硬件开发
评估板
发布信息
The Out-of-Box Experience (OOBE) for the LP-MSPM0C1104 allows interaction with the MSPM0C1104 LaunchPad development kit running its out-of-box demo software.
The LaunchPad implements examples for a blinking LED and button counter.
技术文档
类型 | 标题 | 下载最新的英文版本 | 日期 | |||
---|---|---|---|---|---|---|
产品概述 | 使用 LP-MSPM0C1104 LaunchPad™ 启动整个 MCU 系统 | PDF | HTML | 英语版 | PDF | HTML | 2024年 2月 8日 | |
EVM 用户指南 | LP-MSPM0C1104 评估模块 (Rev. A) | PDF | HTML | 英语版 (Rev.A) | 2023年 12月 14日 | ||
EVM 用户指南 | LP-MSPM0C1104 Evaluation Module User's Guide (Rev. B) | PDF | HTML | 2023年 10月 3日 |